PRESS RELEASE June 3rd, 2016
Echternach - FANUC is pleased to announce the arrival of its new series of Wire Electrical Discharge ma-chines to the European market – the FANUC ROBOCUT α-CiB series. This new ROBOCUT series will replace the previous α-CiA series and is comprised of 3 models: the ROBOCUT α-C400iB and ROBOCUT α-C600iB that were existing models within the range, as well as the new addition, the ROBOCUT α-C800iB. The Euro-pean premiere of the series will be in September at the AMB show in Stuttgart (13-17 September).
Within the new series, the α-C600iB model keeps its previous form, while the α-C400iB has increased its cutting area to X400mm x Y300mm x Z255 with a 500kg workpiece weight capacity.
The newly added α-C800iB model with its cutting area of X800mm x Y600mm x Z310mm and 3000kg work-piece mass capacity will have the smallest footprint in its market range, and is suitable for big press molds and job shoppers.
The FANUC α-CiB machines are compact, high performance wire-cutting machines. The new machines guarantee higher rigidity and cutting accuracy. The symmetrically designed cast iron structure of the ma-chine was optimized for higher stiffness and thermal stability in order to cater for today's high precision needs. FANUC α-CiB are equipped with totally new pulse control (FPC - flexible discharge pulse control).
Software
FANUC ROBOCUT α-CiB machines are operated through the latest Series 31i-WB CNC Control with Touch Screen Technology and are welcoming the new FANUC iHMI user interface. The powerful CNC Control of-fers the most advanced CNC features in control technology and the possibility to operate ROBOCUT CAMi software directly from the CNC screens. The ROBOCUT Linki PC software tool that allows the operator to monitor the machine status in real time will also come with a completely new and user-friendly interface. A quick start-up package (Robot QSP) that allows an easier integration of robots for machine tending is also available for the series.
ABOUT FANUC:
FANUC Corporation, headquartered at the foot of Mt. Fuji, Japan, is manufacturer of FA (Factory Automa-tion), Robots and Robomachines in the world. Since its inception in 1956, FANUC has contributed to the automation of machine tools as a pioneer in the development of computer numerical control equipment. FA-NUC technology has contributed to a worldwide manufacturing revolution, which evolved from the automa-tion of a single machine to the automation of entire production lines. FANUC is committed to developing efficient, reliable and innovative products.
FANUC is the exclusive provider of industry leading FANUC CNC systems and solutions, providing a one-stop shop for comprehensive CNC solutions including industry-leading control systems, a complete range of drives and motors and laser solutions. FANUC also offers engineering support, genuine FANUC parts, repair and factory automation solutions and training programs to machine tool builders, dealers and users.