Food-packaging robots double line speed for Belgium waffle producer
Task: Install six FANUC food-packaging robots equipped with advanced functionality, including iRVision, visual line tracking, load balancing, collision guard and an Ethernet encoder, to pick and place the food (in this case, waffles) on the packaging line.
Solution: The number of pieces of food on the conveyor and their position is communicated to the robots via a camera. The
robot controller, divides the waffles equally among the robots. Using
FANUC’s duo pick feature, each robot grips two waffles and places them on the line, saving time and enhancing transfer speed.
Result: The robotic line is 50 percent faster than the old food processing line. Plus, quality and hygiene has improved. There is also less waste since human operators were prone to breaking off the edges of the waffles, something the robots do not do when packaging delicate food.
Download PDF to find out how food-packaging robots improve efficiency